Hello, dear community.
I am developing a screwing tool and I using an external tool and the UR5e. I am a little confused about the get_tcp_force function.
This is my mockup

Does get_tcp_force return the external force/torque read from the sensor mounted in the robot tool flange?
or
Does get_tcp_force return the forces/torques reader from the force sensor in the tool flange and transform its values to the TCP that has been configured?
It uses the defined TCP but the result is in the Base frame.

To get that in the tool coordinate system, you’ll have to make the transformation:
https://www.universal-robots.com/articles/ur/programming/get-force-and-torque-values-in-tool-coordinate-system/
In the base frame is ok for me.
Do you know the equations that convert the data from the force sensor mounted in the tool flange and the TCP?
Is it also possible to convert those forces to user defined features?
With poses it can be done like this:
Base_TCP = get_actual_tcp()
TCP_Base = pose_inv(Base_TCP)
TCP_Feature = pose_trans(TCP_Base,Feature)
Feature_TCP = pose_inv(TCP_Feature)