I’m currently using our CoBot to measure surface heights. To do so, I lower the Cobot onto the surface until a defined force is reached. I then save the height of the TCP.
At the moment, I am not able to distinguish differences in the region of 0.05 mm by that method.
To clarify, I’m using the force copilot URCap. I give a downward force of 5 N onto the Z axxis, and let the tcp drive a prerecorded path (in which it is standing still, with no force applied). I save the height at the moment it doesn’t change anymore in a seperate thread.
Have I reached the limit of what is possible with the CoBot, or are there other methods to measure objects in a touching manner?
E-series robots have a pose repeatability of 0.03mm for the 3e/5e and 0.05mm for the 10e/16e. With that said, any sort of error in the rest of the system will probably take you out of the range that you are looking for.