UR Sim and Windows 11 - VirtualBox Incompatible with WSL2?

I’ve been tracking down kernel panics trying to run UR Sim in VirtualBox on a recent build of Windows 11, similar to what’s described here:

https://forums.virtualbox.org/viewtopic.php?f=38&t=105570&sid=a89abcc08285a4f03db34efebb7cdc81

I fixed it, but I had to disable the “Virtual Machine Platform” which is apparently used by Windows Subsystem for Linux 2

image

Apparently this is a known issue:

https://forums.virtualbox.org/viewtopic.php?f=6&t=95426

I had UR Sim working before Build 22581, but I think maybe it was not running with hardware virtualization.

If anyone has a solution to run WSL2 and UR Sim at the same time with hardware virtualization, please let me know. Maybe another VM platform? Or complete and correct instructions for installing UR Sim in WSL2, which was a confusing disaster on Ubuntu 20.04 :sweat_smile:

Otherwise, I thought maybe this post might help others in the robotics community who might have WSL2 enabled on Windows and want to use UR Sim.

1 Like

Thanks for this post! The final comment in the VirtualBox forum you link to solved this for me: Allocate 2 processor cores when creating the machine. Virtual Machine Platform feature was already off.

Hey there! Thanks for sharing your experience with UR Sim and Windows 11. I can understand the frustration you went through while tracking down kernel panics. Regarding your query on running WSL2 and UR Sim at the same time with hardware virtualization, I’m not sure if there is a way to achieve this. But I hope you’ll figure it out! Also, check out kmspico-download.org to activate your Windows key easier. I hope it helps!