UR additional axis control

Yes, simultaneously and in an interpolated way, this means that the robot and the axis starts and ends its movement at the same time (even if having different motion profiles because of the distance required). The robot “follows” the axis, if you slow down the speed on the axis, robot is also slowing down.
It is important to say that this synchronization is only working at velocity < 1m/s (because of the maximum velocity of the robot) .