I have two UR robots and they are both on different teach pendants but we would like to go to both of them on the same teach pendant. Does anyone know if you can run two robots off the same teach pendant? We had one collision and we are hoping that if we run them from the same teach pendant that wont happen.
Related topics
Topic | Replies | Views | Activity | |
---|---|---|---|---|
Can you control two Robot with one pendant? | 2 | 599 | January 26, 2021 | |
Can i use the robot without Teach Pendant | 2 | 1297 | January 27, 2021 | |
Can I run Labview via teach pendant? | 2 | 690 | December 21, 2018 | |
Remove teach pendant | 1 | 1896 | September 9, 2019 | |
Is it possible using two ursims in one vmware? | 0 | 399 | January 26, 2022 |