Get rid of teach pendant

Just started working with our new UR20. We’re trying to use it to replace an UR16e on our robot. Our UR16e was an OEM model, and didn’t have a teach pendant. We were kind of in a hurry and bought a “regular” UR20 since there was no OEM model available.

How do we ditch the teach pendant on our UR20? Most importantly, we don’t want to hold down a 3PE button every time we start or use our robot. Also, the pendant is just extra “stuff” when we want to run autonomously. I read something about wiring up an external 3 position switch, but that’s kind of a non-starter too. We just want to turn the robot on and run w/ our existing on/off wireless estop setup. How can we do this with the UR20?

Nevermind. I totally forget about remote mode. I turned that on, and everything seems OK again.

I think from here we remove the teach pendant and wire in our estop, and we’re good. Any reason to think this won’t work?

Hello, how did you manage to utilize the robot without the teach-pendant?

I’m pretty sure he’s using PolyScope 5 and not PolyScope X. I don’t think you can use his experience in your case.

I would make a new thread if I were you.