Stuck in Script Editor after java Exception

Hello,

this happened to me about 3-4 times until now.
Here is how it happened this time:

  1. I tried to run the programm
  2. A spelling mistake (in the script file) was found by the compiler
  3. The Mistake was corrected
  4. Java Exception as shown in the attachement

Perhaps I clicked something to fast and confused the sequence of operations ?

Here are the Images of the failure-codes:

This happened to me in VM and on the teach pendant.
Only way to get out is to close the application.

Perhaps this is also the reason for this topic:

Best Regards,
Alexander Apostolidis