Hi,
is there a possibility to send a quotation mark via socket_send_string()?
I tried " " " but it didn’t work.
Thank You!
Hi,
is there a possibility to send a quotation mark via socket_send_string()?
I tried " " " but it didn’t work.
Thank You!
Try with \ " (without space between) that should result in just the quotation mark
Hi michael,
i tried to allocate a string:="\ “”, but the allocation was not accepted.
I also tried ’ " ', but that also did not work.
Hello,
There currently isn’t a way to do this, however you can accomplish the same task using this workaround: socket_send_string(popup((str_cat("’’",“test”)),"’’")))
where " ’ ’ " - with no spaces is used instead of double quotes.
If you need the quation to be a string to send to some sort of external device you can test: socket_send_string(to_str("’’")) using the same method I mentioned above- " ’ ’ "

Hope this helps.
Hello,
Is it a requirement that you use socket_send_string() to send the quotation? I ask because there’s a support article on the support site (here: How to send a quotation mark via socket communication) that talks about this. Instead it discusses using socket_send_byte() which allows the use of ASCII characters. Hopefully this will help by giving another potential option.
Hi,
thanks inu and dsh for the solutions.
We use Polyscope V3.7, that´s why I cannot use inu`s solution. The string manipulation functionalities are in V3.8.
Socket_send_byte(34) is working for me. I wanted to send data in json-format, to meet the requirements of our customer, a quotationmark is needed in this context.
@jbm and @inu I would like to resurface this question and or propose this for future functionality of Polyscope, I need help sending a double quote ( " ) over socket communication (trying to avoid RTDE). I have tried all three methods listed in this discussion:
The device reads commands/strings as a single line ending in \n. I have used socket_send_line() to communicate with the device and it works fine for most commands even using single quotes within the string.
I can’t share the specific command but let’s say it looks something like this:
String = “Hello World: “URname”, “SomeoneElsesName”,“UR”, “display”, 1”
Socket_send_line(String)
Any help would be great, thanks!
Hi,
I tried your workaround with socket_send_string(to_str(“’’”)), using " ’ ’ " and it looks like it works.
I will send this to an external device at a customer (can’t try right now), but will the device actually see ’ ’ as "? Does to_str() make them into the same character?