SSH port 22 and VNC Viewer timeout

I am getting timeout errors when attempting to SSH and VNC Viewer into a UR10e. This is happening when attempting with a windows laptop and an Ubuntu desktop.

Recently, updated the polyscope 5 software to 5.21.3. The ip address is set to static, which I am able to ping. In Settings → Security → Secure Shell, enable ssh access is checked. Current installed URcaps are UR connect, External Control, and Robotiq grippers.

Is there another setup step I am missing? Or could it be possible interference from a UR cap?