I’m currently reading a value from Cognax camra spreadsheet using the method
telnet_send("GVL10")
and then getting return value and the actual value
receive = socket_read_string() # status code
receive = socket_read_string() # actual cell value
and the problem is that when I try to use it in any way I get type error, for example I’ve tryed to convert the value back to a number but I get an error that is not a string stating with or if I try to convert it to string same error that is not a number
### Read cell value command###
telnet_send("GVL10")
receive = socket_read_string()
textmsg(receive)
receive = socket_read_string()
textmsg(receive)
if to_num(receive) == "1.000":
position = "UP"
end
this is the acutal code, where the telnet_send() function is the one found here
and this is the resoult that I get from the log
1
1.000