Hi folks,
due to the missing function of saving a position in a variable in Polyscope V3.15 I am trying to solve this for an easy setup later.
I thought to use global variables, so the main program can use those variables also. They are all the same syntax. An example is pos_xx. xx is the variable which defines the position.
By asking the user which pos he wants to change I have the pos as an variable. But how can I use this variable to save a position on this variable?
local pActualTCP = p[0,0,0,0,0,0]
xTargetPos = request_boolean_from_primary_client("Is the TCP on point?")
if xTargetPos:
iPosToChange = request_integer_from_primary_client("Which Position do you want to change?")
sPosToChange = to_str(iPosToChange)
sPosToChangeValue = "pos_" + sPosToChange
popup("Is " + sPosToChangeValue + " right?")
get_actual_tcp_pose(pActualTCP)
global 'HERE IS THE PROBLEM' = pActualTCP
popup("That went smooth", title = "Success")
halt
else:
popup("The program will be terminated", title = "Error", error = True, blocking = True)
halt
end