I want to have a program that runs different scripts from different files.
I would really appreciate your suggestions and help.
example:
def main_program():
if (condition_1):
execute_file_1()
elif (condition_2):
execute_file_2()
elif (condition_3):
execute_file_3()
end
end
The subroutine call is what your are looking for.
Use a switch statement to call the cases. Example from my own systems.
@WattsUp
Thanks for the quick reply.
But I’m not so sure if the subroutine is what I’m looking for.
When I’m saving a program into .script the subroutine takes my other file and copies its content in the main program.
As if under the hood it’s still a single file.
To give a bit more context:
I’m trying to write a custom .script driver file.
My problem is that I have two files that control different tools with shared variables with different values.
also, I want to have a script that dynamically calls different files with a string as an input.
Thanks in advance for your suggestions