Hello, I’m using SocketTest to communicate with a UR3 using port 30001 (primary interface). Individual command sending works perfectly

but when I try to send a complete URScript program, it does nothing.
comunication guide
I’ve tried multiple ways of writing that program in a single line, and none worked.
I think the issue is that I’m not distinguishing between lines when writing the different commands because when I tested running the same program in a single script on the actual robot, it only executed the first command and ignored the rest.
My question is: Is there any way to write a complete URScript program in a single line of text, to be able to send it through SocketTest?
Thanks, greetings from Spain