For the RTDE interface can you please provide the return values of runtime_state and their meanings? The documentation only says that it is of the type UINT32 and has the description Program state
I have reverse engineered these states
1 - STOPPED?
2 - RUNNING?
4 - PAUSED?
There is no documentation for this that I have been able to find.
Is there a STOPPING and a PAUSING state?
It is not written about this in documentation in detail.
I defined the following enum.
Stopping : 0
Stopped : 1
Playing : 2
Pausing : 3
Paused : 4
Resuming : 5

Thanks, did you test the remaining states by writing the return value to the console continually and manipulating the PolyScope program state?
Yes, that’s right.
I comfirmed by testing on real robot.(UR3 CB-Series)
Anyway, state is “Paused” when robot is paused and protective stop.
“Resuming” refers to the state in which program is resumed from protective stop.