Recording data with UR Log Viewer

Hi!

I’m trying to use UR Log Viewer to display some GP 32-63 output bit registers, but when I try to select those registers in the generated flightrecord, the GP IO option is not available. I think this option was available in the previous version. I am using UR Log Viewer version: 1.1.0.2.

I attach an image with the flightrecord context menu. As you can see, the GP IO option is not visible.

Is there any other way to do it in this version?

Thanks in advance.

Hi @anon38429663,

the latest UR Logviewer Version is Available here: Universal Robots - Log Viewer V1.2.1.0

In this Version you should have also the GP IO option available you are missing right now.

sko

Thank you, the issue is solved!