Port Accessibility Issues for Gripper Communication on a UR10e Using Sockets and URCaps

Hi, I have already asked this question here (universal robot - Port Accessibility Issues for Gripper Communication on a UR10e Using Sockets and URCaps - Robotics Stack Exchange )
but I think this is the more appropriate forum for my problem.

I’m having trouble controlling a Robotiq EPick Gripper that’s connected to a Universal Robot UR10e.

I followed this guide: Guides — ur_rtde 1.6.0 documentation

Option 3 explains how to communicate directly with the Robotiq URCap through port 63352 using a socket connection. Option 2 talks to the gripper via a serial port mapped from port 54321 of the RS485 URCap running on the robot. However, neither option is working.

The minimal example for Option 3 is not returning from the connect function and Option 2 is failing with the following error:

Modbus Error: No communication with the instrument (no answer)
You can find both scripts below.

Communication through the RTDE interface is working, but I need to control the robot via the ros2 driver during gripper actions, so Option 1 is not applicable.

When I tested the ports with Telnet, I found that they are not exposed by the UR controller.I also looked for settings that could hide the ports, but I couldn’t find any. It is also not possible to connect via SSH or SFTP, even though the settings are enabled in Polyscope.

Any help would be much appreciated.

Option 3


import socket
ROBOT_IP = '192.168.2.2'
PORT = 63351
with socket.socket(socket.AF_INET, socket.SOCK_STREAM) as s:
    s.connect((ROBOT_IP, PORT))

Option 2


import minimalmodbus
import serial
import time


def control_epick_gripper(port, slave_address, command, value=None):
    """Controls a Robotiq ePick gripper over Modbus RTU.

    Args:
        port (str): Serial port (e.g., '/dev/ttyUSB0' or 'COM3').
        slave_address (int): Modbus slave address of the gripper.
        command (str): Command to send (e.g., 'activate', 'grip', 'release', 'set_position').
        value (int, optional): Value for commands that require it (e.g., position, force).
    """

    try:
        instrument = minimalmodbus.Instrument(port, slave_address)
        instrument.serial.baudrate = 115200  # ePick default baudrate
        instrument.serial.bytesize = 8
        instrument.serial.parity = serial.PARITY_NONE
        instrument.serial.stopbits = 1
        instrument.serial.timeout = 1  # Adjust as needed

        if command == "activate":
            # Activation: Set the "Action Request" register (address 0x03E8) to 1.
            instrument.write_register(1000, 1)  # 0x03E8 = 1000
            print("Activating gripper...")
            time.sleep(1)  # Important: Wait for activation to complete
        elif command == "grip":
            # Grip: Set the "Action Request" register (address 0x03E8) to 3.
            instrument.write_register(1000, 3)  # 0x03E8 = 1000
            print("Gripping...")
        elif command == "release":
            # Release: Set the "Action Request" register (address 0x03E8) to 2.
            instrument.write_register(1000, 2)  # 0x03E8 = 1000
            print("Releasing...")
        elif command == "set_position":
            if value is not None:
                # Set Position: Write the desired position to the "Target Position" register (address 0x03E9).
                instrument.write_register(1001, value)  # 0x03E9 = 1001
                print(f"Setting position to: {value}")
            else:
                print("Error: 'set_position' command requires a value.")
                return
        elif command == "get_status":
            # Read the "Gripper Status" register (address 0x03E8)
            status = instrument.read_register(1000)
            print(f"Gripper Status: {status}")
            return status  # return status for further processing if needed
        else:
            print(f"Unknown command: {command}")

    except minimalmodbus.ModbusException as e:
        print(f"Modbus Error: {e}")
    except serial.SerialException as e:
        print(f"Serial Port Error: {e}")
    except Exception as e:
        print(f"An unexpected error occurred: {e}")


if __name__ == "__main__":
    PORT = "/tmp/ttyUR"  # Replace with your serial port
    SLAVE_ADDRESS = 9  # Default ePick slave address

    # Example Usage
    control_epick_gripper(PORT, SLAVE_ADDRESS, "activate")
    control_epick_gripper(PORT, SLAVE_ADDRESS, "grip")
    time.sleep(2)  # Hold grip for 2 seconds
    control_epick_gripper(PORT, SLAVE_ADDRESS, "release")
    control_epick_gripper(
        PORT, SLAVE_ADDRESS, "set_position", 100
    )  # Set position to 100 (adjust as needed)
    control_epick_gripper(PORT, SLAVE_ADDRESS, "get_status")
1 Like

I have managed to solve this problem. I had an incorrectly configured setup of the incoming connections to the robot. You need to specify your IP range and blocked ports in the following menu ‘Hamburger Menu’/Security/General/‘Incoming Connections’.

Source: Universal Robots - Secure setup of UR cobots

For the EPick, you must also connect to port 63352 if you are connecting via sockets.