Is there any way to control the text layout within a popup window?
I query the operator for several dimensions, and would then like to display them so the operator can double-check her entry.
It would be nice to be able to present them in a chart format:
value 1 = 1.5
value 2 = 2.3
etc.
Instead, it just puts them all together, and even strips out leading or following spaces, making it harder to read.
See this post:
It gives an example of using HTML inside the popup string for formatting the text.
Thanks. Was able to insert html breaks and spaces to get this looking like I want.
Also was able to add a header line, as the title line in regular popups isn’t really all that noticeable.