Hi,
I have an application question. With respect to the picture attached. what will be the easiest way to let user to key in a degree and the robot will move the number of degree base on the pivot point? Am i right to say that, if i get the correct TCP, i can use moveC to achieve?
what I would properly have done
- is to set the tcp to the pivot point.
- get the actual tcp pose
- change the angle of this pose
- move to the new pose using movej
- reset the tcp to the tool tcp
Best regards
Hi @hclai77,
welcome to the UR forum ![]()
If you set the TCP in the center of the pivot point, then you can just use a couple of movel:

Hi,
Thanks for a quick response and good illustration.
If the customer just want to specify the angle to be moved respective to this TCP, How should I implement this? Will it be just the movement of rotation in ‘Green’?
Regards,
Lai
You could use function rpy2rotvec to compute the angles for the rotated pose:
set_tcp(p[0, 0, 0.2, 0, 0, 0])
# start pose
pose = p[0.719, -0.026, 0.466, -1.51, 0.50, -0.50]
movel(pose)
# compute rotated pose angles
angles = rpy2rotvec([0, d2r(30), 0])
v1 = angles[0]
v2 = angles[1]
v3 = angles[2]
# go to rotated pose
rotated_pose = pose_trans(pose, p[0, 0, 0, v1, v2, v3])
movel(rotated_pose)