Hello forum and URCap team,
I would like to parse a string in java which contains JSON data such. A sample string could look like this:
String json_str = "{\"field1\":\"val1_str\",\"field2\":\"val2_str\"}"
Using maven, there are various libraries and I prefer to use Jackson Databind (https://mvnrepository.com/artifact/com.fasterxml.jackson.core/jackson-databind).
I included the following dependency in the pom.xml of my URCap:
<dependency>
<groupId>com.fasterxml.jackson.core</groupId>
<artifactId>jackson-databind</artifactId>
<version>2.13.1</version>
</dependency>
I have been following this tutorial: https://www.baeldung.com/jackson-object-mapper-tutorial
Code completion works just fine, syntax errors are found in the IDE and everything compiles and deploys using mvn install -Premote.
But when I restart the robot, the plugin data is not available (no /data/daemon/ directory is available in the respective bundle folder under /GUI/felix-cache/bundle).
I turned everything back and found out, that whenever I use a Java object from this library, the data is broken and the plugin not installed properly.
So my question is:
- How can I include Jackson Databind in the Maven pom.xml and use the JSON parsing from the Java code of my plugin?
- Is there a version conflict of the underlaying Java framework (Robot has Java version 1.6.0_27)?
- Or did I miss anything else?
Best regards,
Steffen