New guidelines for tool mounting torque?

Hi,

the guidelines for fastening a tool to the robot has changed in the new manual (SW 5.14) for UR5e, UR10e and UR16e. The Nm is no longer stated as in previous manual version, which stated: “The M6 bolts must be tightened with 8 N m, strength class 8.8”

Are these still the current guidelines or are there any new ones that we should adapt in our tool manual?