Need help with program flow

I need help with this part of a program. i need to have the cobot go to the start of the program if the part fails. right now if a part fails it rejects and then goes to the next line and continues through the rest of the inspection.

conveyor

MoveJ

Set Laser_Bit_0=Off

Set Laser_Bit_2=Off

Set RH_Trigger=Off

Set LH_Trigger=Off

Above_Conveyor

Waypoint_5

Wait: 0.4

Set LH_Trigger=On

Set RH_Trigger=On

Wait: 1.0

If LH_Laser_Bad or RH_Laser_Bad≟ True

Bef_Above_Bad

Above_Bad_Part

Drop_Bad_Part

Set Vac_1_on=Off

Set Vac_2_On=Off

Above_Bad_Part

Aft_Badpart

Waypoint_1

Set RH_Trigger=Off

Set LH_Trigger=Off

Set Laser_Bit_0=On

Wait: 0.3

Waypoint_6

Wait: 0.6

Set LH_Trigger=On

Set RH_Trigger=On

Wait: 1.0

If LH_Laser_Bad or RH_Laser_Bad≟ True

Bef_Above_Bad

Above_Bad_Part

Drop_Bad_Part

Set Vac_1_on=Off

Set Vac_2_On=Off

Above_Bad_Part

Aft_Badpart

Waypoint_1

MoveL

Drop_Off

Wait: 0.2

Set Vac_1_on=Off

Set Vac_2_On=Off

Wait: 0.2

Above_Conveyor

I have found success using a basic Switch/Case structure, and segmenting the entire process up into “Steps.” Divide your program into smaller pieces and contain each piece into a single Step. Something like this:

image

I know the “if false” is unrealistic, I was just too lazy to name a variable. Use Assignment nodes to write the value of the Switch variable to control the program flow. So at the end of Case 1, I should put “var1 = 2” and from Case 2 I should put Var1 = 3. Case 3 should have an If statement that sets it to 4 (good part, carry on with the rest of the program) or (in my example) 11 to signify the 1st step of a part reject sequence. After the rejection sequence, I set Var1 = 1 to restart.