Hello,
I am testing the example files given in the article “Moving to a position calculated from user input”.
I’ve noticed the following bug at the very end of the article, section “Attached files”:
- example file “square_motion_relative_to_the_tool_with_blends.urp” actually doesn’t correspond to the section “Square motion relative to the tool with blend”. This example file is identical to the first example file “square_motion_relative_to_the_tool.urp”.
Can someone from the UR support team update this article with the correct example file for the the section “Square motion relative to the tool with blend”? Or provide me with a link to download the correct example file?
Thanks in advance for your support.
Regards, Jérôme