Hello everyone,
Is it possible to make interfacing directly via REST or SOAP or something else?
Herewith, I would be grateful if you recommend me which software interface to use for sending the program to the robot and exchange I/O values.
Thanks in advance.
Giorgi
UR controllers are provided with several communication protocols on TCP/IP like Primary Interface, Dashboard Server, RTDE, …
For sending programs, you can either send URScript on the Primary Interface socket or send a program urp file in the robot via SFTP.
See : Overview of client interfaces - 21744
If you don’t want to develop these protocols, you can use a library that does the implementation, like this one.
Thanks a lot.
Another question, is it possible to use 2 interfaces together? For example to send script (the program including waypoints, payloads, etc.) from the primary interface and control the robot real time values (I/O’s, joint position, etc.) via RTDE?
Yes, you can use simultaneously several protocols.
Several clients can even connect to these interfaces at the same time.
Thank you very much.