After halt the program doesn’t return to the start again. Im looking for some script or command to send the robot back to the first line of script and run the program again. I’m in remote control mode and have auto-initialise and auto-start ON, its when the program runs for the first time and meets an IF command resulting a halt. then the program needs to restart, but i cant work out how.
Or a script/command to skip to the last line of the tree, so it will restart automatically.
Solution: “continue” starts from the beginning