Hello, in the script i can see command Direction Until Distance is a thread, is there a limit on how many Untils and thus threads i can put into the program? Is there a difference for cb3 and Eseries?
You can have 50 threads running at one point on the controller. This doesn’t mean you can only have 50 untils, just that you can’t have 50 threads running AT THE SAME TIME.