Hard braking when using moveP

MoveP does not have deceleration since it moves at a constant speed. You can either add a movel to the end as recommended above or use a stopl command following the movep. I think the other issue is unless you do something at the end the movep is going to blended points as well and so may not abruptly stop at the actual end point without either a movel or stopl added.