Feasible Temperature Range for Experiments with Universal Robots

Hi Team,

We are planning to carry out a Tele-Robotic Project with UR5e in an area where the temperature varies from -15 degree Celsius to 5 degree Celsius. Although the temperature in the experimental area vary from 5-21 degree Celsius, the robot may get subjected to -15 degree Celsius during transition from one location to another. We need some help regarding this. Can the technical team throw some light on the packaging aspects of the robot? How much extra insulation and of which type (thermocol, glasswool etc.)should be put inside the existing packaging structure of UR to ensure safe transition? (Note- While working, the robot will be placed in an 5-21 degree Celsius environment)