Hi,
I have build some VIs and call them via Test Stand. First I open connection ->port 29999, I make some movements and tests with the robot then I close the connection. Robot state is now “pause”, waits for the next move.
I restart my Test Stand and labview things, and try to connect again but not possible. I have to restart also the controller.
Why is this happens? Maybe the connection remain open? How to check the connection if it is closed well?
Thanks
Pantelis
Hi @pantelis.volkas,
I’m not sure if I have enough information from your post, but I may be able to help. I have a lot of experience with using the dashboard server in LabVIEW and have developed a toolkit.
Do you have a method to share some screenshots or code? Perhaps, easier if you contact me offline