Hello everyone,
I’m currently working on connecting a UR20 to an Autonics PLC using Modbus TCP/IP. I’ve already managed to link the IP addresses, and on certain addresses I can see data. However, the issue is that this data is not being reflected on the PLC or the robot. At this point, I’m not sure which addresses are actually being detected or mapped correctly.
Has anyone here worked with this type of integration before? If so, could you share an example or some guidance that might help me understand how to properly map the addresses or troubleshoot where the problem could be?
Thanks in advance for any support.