Hi everyone,
I am currently working on trying to connect the UR3e robot with a Raspberry Pi 4 with a ethernet cable. Last month I was able to have success and send code from the Raspberry Pi to the robot but I am not having that same type of success currently. My current process of connecting both is as follows:
- Turn on both UR3 and Raspberry Pi 4 (having an Ethernet cable running into both)
UR3e robot - Activate arm and have it in “Remote” mode. The IP address: 192.168.1.2 and netmask: 255.255.255.0
Raspberry Pi - In a command prompt I enter “sudo ifconfig eth0 192.168.1.2 netmask 255.255.255.0” until there’s a connection. I also ping the IP to make sure there is connection.
- Open Thonny and run my code:
Import urx
rob = urx.Robot(“192.168.1.2”)
After the code I get Tracebacks and a connection refused error. Is there any way to fix this issue or simplify the process if possible? I’m relatively new to all of this so I might be missing something simple.