Hi, I bought a CB-series UR10 and tried the real-time data exchange example from Real-Time Data Exchange (RTDE) Guide - 22229
I have set the IP address of the robot statically to 192.168.1.20.
The problem is that TCP port 30004 is not open. The ssh port 22 is open, but the neither the password easybot nor the password I’ve set in the pendant work (username root).
I would appreciate if someone could tell me if I’ve missed something obvious in the setup.