class ParentNode implements ProgramNodeContribution {
private void addNodes(){
TreeNode root = getRoot();
ProgramNodeFactory nf = getProgramNodeFactory();
try {
for (int i = 0; i <; i++) {
NumberProgramNode numberNode = (NumberProgramNode) nf.createURCapProgramNode(NumberProgramNodeService.class);
numberNode.setNumber(i); //is this even possible?
root.addChild(numberNode)
}
} catch (TreeStructureException e) {
e.printStackTrace();
// See e.getMessage() for explanation
}
}
}
When I create a child node I wish to be able to specify arguments to my child-node, like the example. Is there a way to do this easily? I have made a static variable which counts every time we create a NumberProgramNode, but the problem comes when we create more than one parent-node which can add a child and can remove a child, this behavior will mess the count variable up. So is there a way to send information from the parent-node to their respected child-nodes?
2 Likes