Calibration file in emulator

Hi,
I’m using the UR emulator and I want to access the calibration.conf . I think it is located in the /root/ folder is that right?
.However I cannot access it because permision are denied. Then I try su and use easybot as password but it returns authentication failure. Anyone know which is the correct password??

Thx

Hi,

The calibration.conf file does not normally exist in URsim. You can copy one from a real robot though and it gets placed in the folder /home/ur/ursim-current/.urcontrol

To get to a Linux command prompt within the simulator environment type CTRL-ALT-T and this will get you to a terminal window where you can browse the filesystem and see the directory structure I point out.

Hi following this topic:
Which are the units in the calibration.conf file. Because I see that in the urcontrol.conf.Ur10 the denabit hatemberrs are in meters and radians.

However taking a look at the my calibration file which has these values

delta_theta = [ -9.40498298408416866e-06, 0.27068412154354593, -0.314903939784922426, 0.0442527515792477608, 9.34172007197231709e-06, 5.93755160400425455e-05]
delta_a = [ 4.68164294735672648e-05, 0.0220582008711670552, 0.00158057850161708036, -0.00035922185146348458, 0.000281769745099834986, 0]
delta_d = [ 0.000316664403174682363, 91.8991379508659634, -90.4485183223671356, -1.45123705292539418, -0.000375134660503345652, -0.000216232948727732022]
delta_alpha = [ 0.00031730707235522182, 0.0017812786528813092, -0.0174204031901766219, -0.00145566498545623979, -8.42411731953873755e-05, 0]

is imposible that delta_d is in m since it has values around 90, an also delta_theta in radians it seems to me that has very large values 0.3 radians is like 20º which I think is too much. So I understand the for delta_d and delta_a units are mm and for delta_alpha and delta_theta are degrees. Is that correct?

Hi Mojer,

The units for the calibration config are in m and radian. The first time I saw the values, they didn’t make any sense to me because they seemed too large. I used this procedure to verify the units for the calibration config (I am using UR5)

  1. I got the DH parameters of the UR5 from UR website.
  2. I coded the forward kinematic of the robot using those DH parameters to find the location of the J6 with respect to the base.
  3. I noticed there is a discrepancy between the values of my code and the values I was ready from the UR controller, and when I added the values of the calibration.conf to its corresponding DH parameters, I got exactly the same values as the controller.

This procedure proved me that the units for the calibration.conf are meter and radians, still I have no idea how UR extracted them like this!

I hope it helps.