Steps to reproduce:
1 - Create a pallet node with a 4 points grid pattern on a flat surface aligned with the XY axis of the Cobot base (number of elements tested 2x6 and 4x9)
2 - Inside the toolAction folder teach the point of an Insertion Spiral Node of the force copilot in Z+ tool direction (aligned with Z- base direction)
Expected Behavior:
Insertion function is shifted to insert the picked piece in the correct XYZ position (with Z+ tool pointing downwards)
Actual Behavior:
Insertion function is shifted to insert the picked piece in the correct XY, but Z goes upwards (Z- tool, Z+ base), this effect increases in the elements farther away from the 1st and 4th corneritems (with Z+ tool pointing downwards)
Workaround Suggestion:
- Already tried to insert the Insertion function inside a SubProgram and call it from the Robot Program → Does not work
- Local support suggests is an issue with the points that are not shifted properly in the pallet node
Robot Serial Number:
- 20225200285 UR10e
- 20225500123 UR5e
Affected Version(s):
5.11.0