About the Technical Questions category

Question about UR specs or features? Advanced question about using scripts? Think you may have found a bug? This is the place.

why can’t i post a question?

I want to post a question; how do i do that?

Hello ANBR,

I’ve noticed wrist3 deviation (cyclical wobble-precession) through a 360 degree rotation, which really affects our center probe accuracy setup.
What is the maximum wrist 3 deviation of an UR3.
Am I missing something? New to UR robotics…
Please advise

Thanks

Hi i am having a problem with my ur10 cb3,when im trying to start it,a fault appears
SafetyA:C192A20:Safety system fault:SPI output error detected
Explanation;
Powersupply for the I/O is not detected
how do I fix it?
Thank you

Hello everyone, I need your help

I am working on human-robot interaction control with compliance. I successfully designed and implemented admittance control on the UR robot however, to test the performance of the controller during the robot interaction with human I need to free-drive the robot joints while in remote control mode to show the compliance.

my challenge is that I cant move the robot freely which is difficult to show that the control is working.

please what should I do?

UR10 wrist2 will shake randomly,

I would like to know if for a UR10e robot, the encoder signal decoding frequency marked in the documentation is a maximum value or a minimum value.

i would like to use the conveyor tracking function in my project

Indeed in the doc as you can see it’s marked 40Khz but it’s not very clear to me.

please help