i use UR10
UR software version:3.3.4.310(Dec 06 2016)
s/n:2016303598
if current robot base TCP pose is
x=-349.43mm
y=132.91mm
z=348.32mm
[RPY degree]
rx=179.75
ry=2.92
rz=-83.84
if target rz in RPY degree is 91.716.others pose remain,then wrist3 would turn clockwise to target rz pose
alternate current robot base TCP pose is
x=-349.43mm
y=132.91mm
z=348.32mm
[RPY degree]
rx=179.75
ry=2.92
rz=-98.33
now,the target rz in RPY degree remain 91.716,then wrist3 would turn in anti-clockwise until hit joint limit.
How to avoid this issue?
It sounds like your issue is the same as the problem described here:
There are some suggested workarounds there you can take a look at.