Have an idea for a new PolyScope, URCap API, robot arm, or controller feature? Share it here! Each post should contain only one feature request. ‘Like’ to upvote.
A feature request must have the following format:
- Title of feature request
- Description of feature as use case
As a<role>I would like<this feature>so it can<give some benefit>
E.g. As a UR+ vision system developer, I would like ability to have slider input elements, so it can allow the user easily to adjust contrast and saturation settings within the allowed range. - Optional technical details
E.g. if there are specific technical requirements.
You can also consider elaboration with phrasing like:
- As a “title/function” I would benefit from “feature request” when I “use case”.
- Implementing “feature request” in the URCap API would make it possible to “use case”. Thus making it easier to “practical functionality”.
If you have an alternate use case, to a feature request that already exists in here, please back it up by elaborating on your specific use case. Alternatively LIKE the post, if you believe it is spot on.