I could be wrong but I don’t think you need a generateScript() method in the toolbar contribution. Assuming you are using the ScriptCommand and ScriptSender classes, the following code is something I use to jog the robot from the toolbar:
movePose1.addMouseListener(new MouseAdapter() {
@Override
public void mousePressed(final MouseEvent e) {
if(movePose1.isEnabled()) {
//create a new instance of the ScriptCommand class
final ScriptCommand moveJ = new ScriptCommand();
//create a new String to hold the command
String string = "movej(" + getFavPose1().toString() + ", a=1.4, v=0.30, t=0, r=0)";
//assign the newly created command as Primary. Secondary commands cannot consume robot time
moveJ.setAsPrimaryProgram();
//add the created string to the command
moveJ.appendLine(string);
//create a new instance of a ScriptSender
final ScriptSender sender = new ScriptSender();
//send the created script using the newly created sender
sender.sendScriptCommand(moveJ);
}
}
@Override
public void mouseReleased(final MouseEvent e) {
if (movePose1.isEnabled()) {
final ScriptCommand stopj = new ScriptCommand();
String string = "stopj(2)";
stopj.setAsPrimaryProgram();
stopj.appendLine(string);
final ScriptSender sender = new ScriptSender();
sender.sendScriptCommand(stopj);
}
}
});
I don’t remember exactly where I found these 2 classes. They were somewhere on the forum I think.