UR 10e with Delta PLC- welding

Healthy (System OK)

Robot in Error

Robot at Home Position

Robot Program Selected

Robot Program Call

Robot Program Start

Robot Program Stop

Robot Error Reset

Welding Machine Status

Welding Machine Ready

Welding Machine Error

Welding Machine On / Off Status

Welding Arc On

Welding Arc Fault

(Optional – if you need more signals)

Emergency Stop Active

Safety OK

Servo ON

Cycle Running

Cycle Complete

Please support,for UR creat logical Programming.

If any one done .. Please share me

There’s definitely not enough information here for anyone to help, sorry. What protocol are you using to communicate between the Delta PLC and the UR? What brand welder are you trying to use? Your general approach should be to pick a protocol (ethernetIP, profinet, MODBUS, etc) and make sure both the PLC and welder support that choice. Then find the documentation on the welder that shows which bits/bytes control the signals you’ve listed. Use the PLC to map the UR’s GP Bools and Integers to these appropriate bits/bytes on the welder.