Hi,
I have question regarding trajectory tracking with servoJ and force mode. I need to follow pre-recorded trajectory with force maximum of 30N.
My code looks like this
Program
BeforeStart
zero_ftsensor()
MoveJ
Waypoint_1
Wait: 0.01
joints≔get_actual_joint_positions()
write_output_boolean_register(0, False )
popup("RUN THE PYTHON CODE",title="RUN",blocking= True )
state≔0
Robot Program
write_output_boolean_register(0, True )
sync()
Loop state<3
Loop state≟1
MoveJ
Wait: 0.01
joints
write_output_boolean_register(0,False)
sync()
Loop state≟2
servoj(joints, 0, 0, 0.008, 0.2, 300)
Loop state≟3
end_force_mode()
Halt
sync()
Thread_1
tmp≔p[0,0,0,0,0,0]
Loop
Script: pose_register.script
joints≔get_inverse_kin(p[tmp[0],tmp[1],tmp[2],tmp[3],tmp[4],tmp[5]],get_actual_joint_positions())
sync()
state≔read_input_integer_register(0)
sync()
Thread_2
force_mode_set_damping(0.1)
force_mode(tool_pose(),[0,0,1,0,0,0],[0.0,0.0,30,0.0,0.0,0.0],2,[0.15,0.15,0.15,1.57,1.57,1.57])
sync()
Problem is that robot is not following path as is should in Z axis.



As you can see from my plots robot is not following trajectory in Z axis (Y and X are correct). Approximately at time-stamp of 900 you can see contact with surface. My question is how to make the robot follow the path with maximum of speed of 0.15m/s and maximum of force of 30N (± 10N). Damping and gain scaling parameters are not doing the trick.
I saw already some implementations of updating wrench parameter in force_mode() based on PD controller but I need to apply stable 30N.
Any suggestions ?
Thanks ![]()