Hello,
I want to build a Visual Basic Program where I will send over ethernet positioning data.
How can I do this? Is there a special syntax to get data sent over Ethernet?
Thanks
Hello,
I want to build a Visual Basic Program where I will send over ethernet positioning data.
How can I do this? Is there a special syntax to get data sent over Ethernet?
Thanks
It is possible to sending script into primary interface with the socket.
There are different ways , the most simple one i think is with primary interface , i made this small code . Basicly if you send any UR command with s.send + encode utf8 at the end , it should understand it.
But remember that robot doesn´t return anything , so when you send a pose , python doesn´t know when the pose is reached. It´s not the bets way , but it works.
import socket
import time
HOST = “192.168.101.15”
PORT = 30002
s = socket.socket(socket.AF_INET, socket.SOCK_STREAM)
s.connect((HOST, PORT))
#s.send ((“movel (p[0.35963,-0.37947,0.03807,0.0,0.0,5.498], a=0.2, v=0.1)”+“\n”).encode(“utf8”))
#time.sleep(6)
#s.send ((“movel (p[0.35963,-0.37947,0.43807,0.0,0.0,5.498], a=0.2, v=0.1)”+“\n”).encode(“utf8”))
#time.sleep(6)