RTDE script_control_line

Good morning,

I have a Question regarding the script_control_line output from the RTDE Interface. The documentation is a bit confusing about this:

Script line number that is actually in control of the robotgiven the robot is locked by one of the threads in the script.

If no thread is locking the robot this field is set to ‘0’. Script line number should not be confused with program tree line number isplayed on polyscope

I expected that this number reflects the program progress in some way. But essentially it seems to be always 0. I tried a normal running program in polyscope, a script send to the primary interface and interpreter mode. but nothing seems to have any effect on this number.

Could someone explain what this is for?

Thanks and best regards
Jan