Problem with inaccessible targets in RoboDK program for UR10 robot

Hello everyone,

I’m working with RoboDK on a trajectory planning process for a UR10 robot with the goal of creating a series of targets around a central point. My code calculates each target using virtual angles and positions the robot accordingly. Even though I used SolveIK to calculate the joint arrays needed and MoveJ_Test to check the reachability of each target before adding it to the program, I still have targets that show an “Unreachable target” warning in RoboDK.

I am using Python code in Pycharm. The code includes:

Using SolveIK to calculate joint positions.
Testing if MoveJ_Test returns a value of 0, indicating that movement is possible.
If the target is unattainable, the code skips it and prints a warning.
Has anyone encountered a similar problem or can recommend another way to check accessibility before adding the target?

Thanks in advance!

It looks like your RoboDK UR10 targets are out of reach due to joint limits or tool settings. Check your tool frame and workspace range. Also, consider grabbing a Windows 10 or 11 key from Digitlogs for better system performance.

thank you for your respawn.
is there a way to check the workspace range?