I discovered a Null Pointer Exception in Polyscope 5.20. The error occurs after a safety stop of the robot, when attempting to save or start the program afterward. The only solution is to restart the robot. It is likely related to the palletizing function.