Hello,
I am currently working on developing a urcap for my application. I have successfully created a drop down menu for selection in the Installation Node, but on the selection of certain parameter i am unable to send the data back. How do i do this?
In the program node, it is easy to do it with and there are several examples of it, but in the installation node, i am unable to find such example too which returns the data after selection. Anyone with an answer for this?
Thanks.
Hello vinneth1,
i’m not quite sure if I understood your problem to the full extend. As far as I know you can create such a combobox just the same way as in the ProgramNode. Just make sure to use the InstallationNodeContribution instead of a ProgramNodeContribution.
You could take a look at how it’s done in the ProgramNode in this tutorial.:
https://plus.universal-robots.com/getting-started/myfirsturcap-creating-the-view/
Hello Lutter,
I cannot do this way because i do not use the ContributionProvider class. If i have to do that way, then i have to redo everything. I could create the combobox in the installation node, and i could see the drop down menu also. But upon a certain selection of the combobox items, i need to update the combobox items.
For eg:
Box box = Box.createHorizontalBox();
box.setAlignmentX(Component.LEFT_ALIGNMENT);
JLabel label = new JLabel(" digital_out ");
combo.setPreferredSize(new Dimension(104, 30));
combo.setMaximumSize(combo.getPreferredSize());
combo.addItemListener(new ItemListener() {
@Override
public void itemStateChanged(ItemEvent e) {
if(e.getStateChange() == ItemEvent.SELECTED) {
//provider.get().onOutputSelection((Integer) e.getItem());///( How do i get this command with normal class and not using Contribution provider?)
}
}
});
box.add(label);
box.add(combo);
return box;
I could do all the commands except the provider.get() how do i do that? Thanks again
You don’t need to use a ContributionProvider in the InstallationNode. You can directly link your InstallationNodeContribution inside your InstallationNodeView.
Here is an example of a similar function inside the view:
private Box createFunctionalityEnabledBox(String text, final TCIInstallationNodeContribution contribution) {
Box box = Box.createHorizontalBox();
box.setAlignmentX(Component.LEFT_ALIGNMENT);
CHECKBOX_FUNCTIONALITY_ENABLED.setText(text);
CHECKBOX_FUNCTIONALITY_ENABLED.addActionListener(new ActionListener() {
@Override
public void actionPerformed(ActionEvent e) {
contribution.userSelectedFunctonalityEnabled(CHECKBOX_FUNCTIONALITY_ENABLED.isSelected());
}
});
box.add(CHECKBOX_FUNCTIONALITY_ENABLED);
return box;
}
Also make sure to link your contribution in the BuildUI method.
@Override
public void buildUI(JPanel panel, TCIInstallationNodeContribution contribution) {
panel.setLayout(new BoxLayout(panel, BoxLayout.Y_AXIS));
panel.add(createFunctionalityEnabledBox("Test", contribution));
I hope this helps you out.
Best Wishes,
Florian
Hello Florian,
I tried the code above, it does not work. May i know what is CHECKBOX_FUNCTIONALITY_ENABLED?
This code snippet doesn’t work as is. It’s from one of my projects. It’s supposed to give you a concept of how it’s done for your code, not to run it as is.
Your line:
Should be replaced with: contribution.onOutputSelection((Integer) e.getItem());
Also you need to change the Declaration where you define your combobox to accept a InstallationNodeContribution as argument instead of a ContributionProvider. Similar to:
private Box createFunctionalityEnabledBox(String text, final TCIInstallationNodeContribution contribution) {
Also in BuildUI you need to hand over the contribution instead of the provider.
I hope this helps.
Hello Florian,
It worked. Thank you so much for the help.