Hello everyone,
I am having occasional problems in the RTDE communication. I use @osh Java implementation and the issue may be related to this one from @mbush.
I have many output variables configured and 8 input variables, specifically 8 variables of type INT32
(input_int_register_X
). Checking the console with CTRL+ALT+F10, I can see the following warning message: WARNING - RTDE Input buffers full.
Any suggestions on how to solve this? Are the number of inputs limited to a maximum size?
Thank you.
Resolved. The problem was that I was updating the inputs at a too high frequency (125Hz, or 8ms). By using a lower frequency (10Hz, or 100ms), like the one in the example code, the problem has disappeared.
It seems to be a problem with buffer overrun.
See the answer to the question here:
The bad news: Lowering the frequency may only delay the problem
Ups!
Wrong post. Sorry