Hi everyone,
I am currently working with PolyScope X (version 10.11.0) and I’m looking for a way to start a program from a specific line or waypoint, similar to how it was possible in PolyScope 5.
I’ve noticed that I can use breakpoints and the ‘Step’ button to go through the program line by line, but is there a way to directly select a line in the program structure and begin execution (‘Play’) from that point without running the previous sections?
If this feature is not yet natively available in the UI, are there any workarounds or plans to implement a ‘Play from selection’ feature in future updates?
Thanks in advance for your help!