How do you make your light flash to show green flashing on tower light with Universal Robot?
Tie an output from the robot to the ON input of your green light. Then use a Thread like so:

Interesting idea. Hadn’t though of that. You could create logic that sends various signals to the light based on what the robot does. ![]()
I made a script that can flash any DO or CO at a variable rate. It ends up looking something like:

The second parameter is kinda weird, in that it’s a binary position of an integer, not a “period in seconds” type of thing. So for example, putting in a 2 flashes it twice as slow as 1, and 3 is twice as slow as 2, and so on. I’m sure it can be modified to take seconds as the argument instead, but it was a pretty elegant solution for me, since I just needed a “flash fast or slow” type thing.
Found it on my computer, so I’ll include it below. As with most of what I write, I barely remember what I was doing at the time, I just know the functions do what they say lol.
enableDOFlash = [False,False,False,False,False,False,False,False]
DOFlashRate = [0,0,0,0,0,0,0,0]
enableCOFlash = [False,False,False,False,False,False,False,False]
COFlashRate = [0,0,0,0,0,0,0,0]
def startFlashDO(outputNumber, rate):
enableDOFlash[outputNumber] = True
DOFlashRate[outputNumber] = rate
end
def stopFlashDO(outputNumber):
enableDOFlash[outputNumber] = False
set_standard_digital_out(outputNumber, False)
end
def startFlashCO(outputNumber, rate):
enableCOFlash[outputNumber] = True
COFlashRate[outputNumber] = rate
set_configurable_digital_out(outputNumber, False)
end
def stopFlashCO(outputNumber):
enableCOFlash[outputNumber] = False
end
thread flasher():
count = 0
while(True):
global flashArray = integer_to_binary_list(floor(count))
i = 0
count = count + 1/500
if(count >= 50000):
count = 0
end
while(i <= 7):
if(enableDOFlash[i]):
DOflashIndex = DOFlashRate[i]
set_digital_out(i, flashArray[DOFlashRate[i]])
end
if(enableCOFlash[i]):
COflashIndex = COFlashRate[i]
set_configurable_digital_out(i, flashArray[COFlashRate[i]])
end
i = i + 1
end
end
end