Hi try to generate some initial code using generateScript, at first I added the code to my installation-node, but the code wasn’t generated if you didn’t click on the installation node.
The other idea was that I added a simple bool checking if the code has already been generated:
if(!initialized){
generateInitScript();
}
the only problem using this way, is that I need to know when the program has ended, so that i can set
initialized = false.
I want to know if there is a way of generating a certain script once, or do I need to use the dashboard server to look up the state?
I solved this quite simple, I created a static class with an id counter 
example below:
public class ProgramNodeCounter {
public static ids = 0;
}
public class FooProgramNodeContribution implements ProgramNodeContribution {
private int currentId;
public FooProgramNodeContribution(){
ProgramNodeCounter.ids++;
currentId = ProgramNodeCounter.ids;
}
@Override
public void generateScript(ScriptWriter scriptWriter){
if(currentId == 1){
generateInitScript(scriptWriter);
}
}
}
Only problem is when you begin to delete the node.