Hi guys!
I’ve got a question about a centering application. I appreciate all your help!
appreciate all your help!
Details:
I have a UR10 e-Series and an RG2 gripper on it. There’s an optical sensor on the fingertips. I have to identify the center of a transparent glass jar, without touching it.
The problem:
When I start the centering with the jaws open:
1.) Move sideways towards the jar, I get the first “HI” state from the sensor. (get_actual_tcp)
2.) Move further until I wait for the ‘LO’ status at the end of the neck of the jar. (get_actual_tcp)
The problem is that I get false ‘LO’ status because of the transparency of the jar. What sequence should I use to consider only the last ‘LO’ signal, instead of the current one?
Thanks a lot in advance!